Empty Pipe Detection

Empty Pipe Detection

Switch empty pipe detection on and off
Empty Pipe Detection parameter properties
Property
Value
Selection / Range
  • Off
  • On
Factory Setting
Off
*Depends on order options or device settings
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

New Adjustment

Select type of adjustment
New Adjustment parameter properties
Property
Value
Selection / Range
  • Cancel
  • Empty pipe adjust
  • Full pipe adjust
Factory Setting
Cancel
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Switch Point Empty Pipe Detection

Enter hysteresis in %, below this value the measuring tube will detected as empty
Switch Point Empty Pipe Detection parameter properties
Property
Value
Selection / Range
0 - 100 %
Factory Setting
50 %
*Depends on order options or device settings
Visibility
Operator
Write Access
Maintenance
Data Type
FLOAT

Response Time Empty Pipe Detection

Enter the time before diagnostic message S862 ''Pipe empty'' is displayed for empty pipe detection
Response Time Empty Pipe Detection parameter properties
Property
Value
Selection / Range
0 - 100 s
Factory Setting
1 s
*Depends on order options or device settings
Visibility
Operator
Write Access
Maintenance
Data Type
FLOAT
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal