Custom Input Connection

Input Assembly Positions 1-10

Assignment of process variable to positions 1-10 of the custom input data.
Input Assembly Positions 1-10 parameter properties
Property
Value
Selection / Range
  • Off
  • Volume flow
  • Mass flow
  • Corrected volume flow
  • Flow velocity
  • Conductivity
  • Corrected conductivity
  • Temperature
  • Electronic temperature
  • Totalizer 1
  • Totalizer 2
  • Totalizer 3
Factory Setting
Volume flow
*Depends on order options or device settings
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16

Input Assembly Positions 11-20

Assignment of process variable to positions 11-20 of the custom input data.
Input Assembly Positions 11-20 parameter properties
Property
Value
Selection / Range
  • Off
  • Actual diagnostics
  • Previous diagnostics
  • Mass flow unit
  • Volume flow unit
  • Corrected volume flow unit
  • Temperature unit
  • Conductivity unit
  • Unit totalizer 1
  • Unit totalizer 2
  • Unit totalizer 3
  • Verification results
  • Verification status
Factory Setting
Volume flow unit
*Depends on order options or device settings
Visibility
Operator
Write Access
Maintenance
Data Type
ENUM16
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal