Configuration
Add-on-Profile (AOP)
The module functionality is configured through a custom, separately-installable
Add-on-Profile within RSLogix 5000 Software. When a module from the RSLogix 5000 Select
Module dialog is added to the project tree, the following items are created in the
project:
- a custom Module-Defined Data Type, and corresponding Input, Output Tags
- a producer/consumer IO connection using the modules specific IO assemblies and sizes.
DIP Switches for hardware addressing
The IP address of the measuring device can be configured for the EtherNet/IP network using
the DIP switches. Addresses in the range from 0 to 254 are permitted (the address 255 is
reserved for the broadcast address).
The IP address for software addressing is active when the device leaves the factory
(default IP address: 192.168.1.212), i.e. all the DIP switches for hardware addressing are
set to OFF.
Switches 1-8 configure the last three digits (last octet) of the IP address. The first
three octets can be configured via software addressing to reflect the desired hardware IP
address.
Setting the IP adress with switches

Provide Feedback