Diagnostics
Global - Device Name
(class 0x310, instance 1, attribute 27)
Type of the product.
Global - Status Signal
(class 0x310, instance 1, attribute 144)
Global - Device Tag
(class 0x310, instance 1, attribute 1)
Current - Module
Slot in which the Module is located. Sampler, Software and Analyzer are virtual
modules.
Value | Slot |
|---|---|
0 | Slot 1 |
1 | Slot 1 |
2 | Slot 2 |
3 | Slot 3 |
4 | Slot 4 |
5 | Slot 5 |
6 | Slot 6 |
7 | Slot 7 |
8 | Sampler |
9 | Software |
10 | Analyzer |
Current - Port
Number of connector on the extension module.
Current - Status Signal
Diagnostic category according Namur NE107 definition.
Value | Status category |
|---|---|
0 | Ok |
1 | Failure |
2 | Function Check |
4 | Maintenance required |
8 | Out of Specification |
Current - Diagnostic Code
See the product manual for a list of diagnostic codes and remedy information.
Current - Date
Date the diagnostic event was raised.
Current - Time
Time of day the diagnostic event was raised.
Last - Module
Slot in which the Module is located. Sampler, Software and Analyzer are virtual
modules.
Value | Slot |
|---|---|
0 | Slot 1 |
1 | Slot 1 |
2 | Slot 2 |
3 | Slot 3 |
4 | Slot 4 |
5 | Slot 5 |
6 | Slot 6 |
7 | Slot 7 |
8 | Sampler |
9 | Software |
10 | Analyzer |
Last - Port
Number of connector on the extension module.
Last - Status Signal
Diagnostic category according Namur NE107 definition.
Value | Category |
|---|---|
0 | Ok |
1 | Failure |
2 | Function Check |
4 | Maintenance required |
8 | Out of Specification |
Last - Diagnostic Code
See the product manual for a list of diagnostic codes and remedy information.
Last - Date
Date the diagnostic event was raised.
Last - Time
Time of day the diagnostic event was raised.
Provide Feedback