Configuration Parameters

Webserver Enable

(class 0x310, instance 1, attribute 3)
Use this parameter to enable or disable access to the webserver in the device. If you cannot reach the webserver, please check first whether the device is reachable over the network using the "ping" command. If you cannot reach the device using the "ping" command, please contact your networt administrator to check whether the network is configured correctly and an IP-route to the device webserver exists.
Webserver enable encodnig
Value
Webserver enable
0
ON
1
OFF

Open Configuration

Press this button to open the configuration webpage of the device with your default webbrowser.
The webbrowser will load a javascript application which allows remote operation of the device display. During remote operation the local operation is temporarily disabled to prevent simultaneous changes to the device parameterization. The local operater can retake the operation anytime from the webbrowser.

Open Logbooks (*.dat)

Press this button to open a webpage with your default webbrowser, which contains URL links to different logbooks in *.dat file format. These files can be imported into the Field Data Manager software available from Endress+Hauser.

Open Logbooks (*.csv)

Press this button to open a webpage with your default webbrowser, which contains URL links to the logbooks in *.csv file format. You can save these files to disk and open it with any text editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal