Documentation

Manual

The primary sources of detailed module information is the Liquiline CM44xx EtherNet/IP manual. It can be found on the CD or on the Endress+Hauser website (www.endress.com).

EDS File

The EDS file is used for identifying the module to network tools, such as RSLinx, RSNetWorx or a CIP (refer to "CIP" in RSLogix5000 HELP) network browser (e.g. RSLinx Who). It can also be downloaded from the Endress+Hauser website. The EDS file is installed using the RSLinx Hardware Installation Tool. The EDS file can also be directly loaded from the device using RSLinx.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal