Sample Projects
Sample programs are available for download from the AMCI website at www.amci.com Sample projects for some modules are also shipped with RSLogix 5000; select "Vendor Sample Projects" on the main RSLogix 5000 help menu.
NOTE: Prior to the availability of add-on profiles, sample projects for modules used the 1756 generic module profile (1756-MODULE). Those sample projects need to be modified for use with an AOP.
Provide Feedback