Servers view
Use the
Servers
view to enable and disable the TCP and UDP ports that are used by the
device when it acts as a server. EtherNet/IP uses TCP/IP or UDP/IP for communication.If the device profile is online to a configurable TCP or UDP server, use the settings to:
- Enable or disable the port.
- View information about the TCP or UDP port.
- Refresh communication to obtain the latest port information from the device.TIP:The information in theServersview is only available when online and configurable ports are available.
Provide Feedback