Points view parameters (output devices)

The
Points
view for the output devices includes these parameters:
Parameter
Description
Point
Displays the point number to which this configuration applies.
Output State During
Program Mode
Determines the behavior of each output when the controller transitions to Program mode. While in Program mode, outputs from the controller are ignored and the output behaves according to these:
  • Off
    - Output is 0 or Off
  • On
    - Output is 1 or On
  • Hold
    - Output maintains last state
Output State During
Fault Mode
Determines what happens to the output of each point after a communication fault occurs and the device enters Communications Fault mode.
  • Off
    - Output is 0 or Off
  • On
    - Output is 1 or On
  • Hold
    - Output maintains the current level
Fault Mode Output State
Duration
Determines the length of time the Fault Value value is held prior to the Final Fault State.
Tip: This parameter is not supported for the 5069-OW4I and -OX4I devices.
Fault Mode Output State
Final State
Determines whether the device transitions to On or Off after the Fault Mode Output State Duration elapses. The default final state is Off. If you choose Forever for Duration, you cannot choose a final state. The device retains its current Fault mode state.
Tip: This parameter is not supported for the 5069-OW4I and -OX4I devices.
Output State When Communications Fail in Program Mode
Determines the output action if communication fails in Program Mode.
  • Leave outputs in Program Mode State
  • Change outputs to Fault Mode State
Enable No Load Diagnostics
Determines whether No Load detection is enabled. No Load detects whether a signal wire has been disconnected from one of its terminals or the RTB has been removed.
Diagnostics
Opens
Ptxx Diagnostics
for diagnostic information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal