Configure the points for an output device
Configure point properties for the output devices.
To configure the points for an output device
- On the tab for the device, selectPoints.
- In thePointsview, fill in the parameters and selectOK.
Provide Feedback