Points view parameters (input devices)
The
Points
view for the input devices includes these parameters:Parameter | Description |
|---|---|
Point | Displays the point number to which this configuration applies. |
Input Filter Time Off -> On | Defines how long an Off to On input transition must remain in the On state before
the device considers the transition valid. |
Input Filter Time On -> Off | Defines how long an On to Off input transition must remain in the Off state before
the device considers the transition valid. |
Provide Feedback