Configure the points for an input device
Configure point properties for the input devices.
To configure the points for an input device
- On the tab for the device, selectPoints.
- In thePointsview, fill in the parameters and selectOK.
Provide Feedback