Events view parameters
The
Events
view includes these parameters:Parameter | Description |
|---|---|
Event | Shows the event number to which this configuration applies. |
Enable Event | Shows whether the corresponding event trigger is active. Events are triggered once
conditions match the event definition. |
Latch Event | Shows what happens to the current event when a new event is received. When this parameter is selected, events are latched until acknowledged. A new event
is lost if the previous event has not been acknowledged. When this parameter is not selected, new events overwrite old events. |
Provide Feedback