Configure system power alarm properties
Configure the alarm properties to trigger the system power alarms when system power exceeds
high or low voltage limits.
To configure system power alarm properties
- On the tab for the device, selectAlarms.
- In theAlarmsview, selectEnable System Power Alarmsif it is not already selected to enable the system power alarms.
- In theHigh System Power Alarm Limitbox, enter the maximum voltage allowed before the high system power alarm transitions from off to on.
- In theLow System Power Alarm Limitbox, enter the minimum voltage allowed before the low system power alarm transitions from off to on.
Provide Feedback