Notch filter
The notch filter is a built-in feature of the Analog-to-Digital Converter (ADC) that
attenuates noise at a specified frequency. The specified frequency could be on a line or set
to another value. The notch filter reduces the amplitude of the signal with minimal signal
distortion.
Choose a notch filter based on what noise frequencies are present in the device operating
environment and any sampling requirements that are needed for control. For example, if the
notch filter setting is 60 Hz, 60 Hz AC line noise and its overtones are attenuated.
For more details, see the
5000 Series Analog I/O Modules User Manual,
publication
number 5069-UM005
.Provide Feedback