Calibration mismatch
Performing calibration can cause unexpected results if:
- At least one channel is selected, and
- There is a mismatch between the device listed in the application and the actual physical device, and
- The system is active.
It is strongly recommended that you select
No
, check the
configuration, and shut down the system before performing calibration.Provide Feedback