Unable to launch RSNetWorx for EtherNet/IP program file

Unable to launch RSNetWorx for EtherNet/IP. An error occurred when locating RSNetWorx for the EtherNet/IP program file or executing it. Refer to the error dialog box for the exact cause of the error.
If this problem continues, launch RSNetWorx for EtherNet/IP manually by using the
Start
Program
option.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal