Data Types

Define any literal, expression, or variable used in a program organization unit (POU) by a data type. Apply data type coherence in graphic operations and literal statements. Program objects using these elementary IEC 61131-3 types:
  • BOOL: logic (true or false) value
  • DINT - Integer: 32-bit integer value
  • REAL - Real: 32-bit real (floating) value
  • TIME: time values up to 23h59m59s999ms. These value types cannot store dates
  • MESSAGE: character string having a defined size that represents the maximum number of characters the string can contain. In the dictionary instance, set
    StringSize
    to the maximum character length.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal