Tree view for defined word cross references
The
References
pane displays additional information for the cross references of a defined word graphically from the Tree view.
Item | Name | Description |
|---|---|---|
![]() | Common path | The common path of the defined word selected in the Elements pane and the number of cross references. |
![]() | Program organization unit (POU) | The name of the POU using the defined word and the quantity of cross references. |
![]() | Used by | The defined word is used by the POU. |
![]() | Defined word | Name of the defined word. |
![]() | Location | Location of the cross reference in the language editor grid. |
![]() | Element | Element affected by the cross reference. |
Provide Feedback