Import Selected Environment Settings
When importing selected environment settings, choose a file containing the settings to import, then select the required settings to import from the list of available environment settings in the file. Environment settings identified with a warning symbol are not selected by default since these may contain intellectual property or sensitive information. Some categories may have sub-categories visible upon expanding the arrows to the left of the category item.
The settings importation process requires these operations:
- Choose whether to save the current environmental settings or overwrite the current setting with the settings to import.
- Choose a file containing the collection of environmental settings to import.
- Select the individual settings to import from the list of available environment settings in the settings file.
During the environment settings import process, a dialog indicates the progress of the operation. Upon completion of the environment settings import process, a summary page shows the results of the operation.
Provide Feedback