Export Selected Environment Settings

When exporting selected environment settings, choose the settings to export from the list of available environment settings. Environment settings identified with a warning symbol are not selected by default since these may contain intellectual property or sensitive information. Some categories may have sub-categories visible upon expanding the arrows to the left of the category item.
The settings exportation process requires the following operations:
  1. Choose environment settings to export.
  2. Name a settings file.
During the environment settings export process, a window indicates the progress of the operation. Upon completion of the environment settings export process, a summary page shows the results of the operation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal