The manufacturing sector is embracing a transformation, driven by the necessity for enhanced resilience and operational efficiency in the face of recent global disruptions.
A vast majority of manufacturers surveyed for our State of Smart Manufacturing Report (81%) say the obstacles they face—both within their organization and externally—are accelerating digital transformation. This number rises above 90% in certain APAC regions such as India and Japan.
Facing persistent challenges like inflation, rising energy costs, cybersecurity risks, and skills shortages, manufacturers view technology—particularly cloud platforms—as a highly effective mitigation strategy.
Investments reflect this, with cloud/SaaS and AI consistently ranked as the top two technology investments, with cybersecurity and quality rounding out the top four spots according to the 2025 report.
Ultimately, the cloud is the bedrock upon which the modern, agile, and resilient connected enterprise is built.