Rockwell Automation has recently added the option to implement OPC UA within our communication portfolio. We’ve configured this update to enable a more secure and stable interface to 3rd Party Servers and Clients with ease. Join speaker Alan Sanders during this webinar as he demonstrates the simplicity at which these options can be configured and included within your application.
Key Takeaways:
1. How Rockwell Automation's Communication Offering is changing.
2. What new features are available for me within FactoryTalk Linx.
3. How OPC UA is configured as a server or client.
-Yes one PDH credit