Loading
Innovation Center LOGO
Recent ActivityRecent Activity

Kinetix Premier Integration

The step-by-step process to Premier integration between Kinetix drives and Logix controllers in one platform, simplifying motion setup, diagnostics, and replacements for peak efficiency. - [Implementation time: 60 Minutes]
Innovation Center Home Page
A man interacts with a tablet to manage a machine, highlighting the use of digital devices in operational tasks.
Innovation Center LOGO
  • Overview
  • Installation Guide
  • Downloads
  • Contact us
  • I want to subscribe.
Innovation Center Home Page
 

What is this for?

Premier integration from Rockwell Automation enhances motion control by enabling Kinetix drives and Logix controllers to work natively within an integrated design environment. Using a single software to configure both simplifies axis programming, synchronization, and motion profile management, while configurations are automatically stored in the controller.

This integration provides advanced diagnostics for predictive maintenance, improved visualization through pre-engineered graphics, and automatic device configuration, reducing downtime by restoring firmware and parameters after replacements. The result: an optimized motion solution that boosts efficiency, reliability, and customer productivity.

 

Is this useful to me?

This is useful because Premier Integration between Kinetix drives and Logix controllers delivers key benefits for motion control applications:

  • Simplified design and programming: A single software to configure controllers and drives reduces time and errors.
  • Precise synchronization and profile management: Ideal for multi-axis systems and complex applications.
  • Advanced diagnostics and predictive maintenance: Detect issues before failures occur, preventing unplanned downtime.
  • Enhanced visualization: Pre-engineered graphics make operation and monitoring easier.
  • Automatic device configuration: Minimizes downtime when replacing drives by restoring firmware and parameters without manual intervention.

 

Application areas - Food, Manufacturing, Beverage

AHIC Download ICON VF.png

Downloads

Please note: You will need to agree to the Terms & Conditions for each download.

Downloadable file ›
Legal Disclaimer Acceptance. ROCKWELL AUTOMATION WILL PROVIDE ACCESS TO ROCKWELL PRODUCTS (BEST PRACTICES, APPLICATIONS AND KNOWLEDGE) ON THE CONDITION THAT YOU ACCEPT AND COMPLY WITH THE FOLLOWING TERMS AND CONDITIONS. YOU ACCEPT AND AGREE TO BE BOUND BY THE TERMS OF THIS AGREEMENT BY DOWNLOADING, INSTALLING, COPYING, OR OTHERWISE USING PRODUCTS. IF YOU ARE ACCEPTING THESE TERMS ON BEHALF OF ANOTHER PERSON, COMPANY, OR OTHER LEGAL ENTITY, YOU REPRESENT AND WARRANT THAT YOU HAVE FULL AUTHORITY TO BIND THAT PERSON, COMPANY, OR LEGAL ENTITY TO THESE TERMS. IF YOU DO NOT AGREE TO THESE TERMS, DO NOT DOWNLOAD, INSTALL, COPY, ACCESS, OR USE THE PRODUCTS, SOFTWARE AND/OR CLOUD SERVICES. 1. Rockwell Automation retains full ownership and title to all Products and related documentation. No rights or licenses are granted other than those set forth in this Agreement. Company grants to Rockwell Automation a non-exclusive, worldwide, royalty-free, perpetual, non-revocable license to use any feedback Company provides regarding the Products, even if Company has designated the feedback as confidential. Rockwell Automation will be entitled to use the feedback without restriction or compensation to Company. 2. Company may not lease sub-lease, assign, license, sub-license or otherwise transfer any of the Products without the prior written consent of Rockwell Automation. Company may not assign or otherwise transfer access rights to the Products without the prior written consent of Rockwell Automation. Any reverse assembly, reverse engineering, decompilation, and creation of derivative works based on the Products by Company is prohibited. 3. Company acknowledges that Products provided under this Agreement are Rockwell Automation’s Confidential Information and are covered by effective or pending copyrights, patents, trademarks and/or trade secrets of Rockwell Automation, and Company agrees to maintain confidentiality by not disclosing Products or documentation to any third party without the prior written consent of Rockwell Automation and to protect the confidentiality of the Products as it would Company’s own confidential information. Company agrees that its obligation of confidentiality under this paragraph shall survive expiration or termination of this Agreement. 4. Company agrees that Products provided under this Agreement are prototypes and examples and its application and results may vary depending on each customer and project conditions. Rockwell Automation do not warranty the same results. This Agreement shall in no way be construed as a commitment by Rockwell Automation at any time to manufacture and/or offer Products for sale. There is no explicit or implicit service level agreement associated with using the Products. Rockwell Automation does not warrant that the functions contained in the Products will meet Company’s requirements. Company agrees to use all Products only in accordance with the instructions and only for the intended usages identified in the documentation. 5. EXCLUSION OF WARRANTIES AND LIMITATION OF LIABILITY. THE PRODUCTS ARE PROVIDED "AS IS". ROCKWELL AUTOMATION DISCLAIMS ANY AND ALL WARRANTIES, EXPRESS, IMPLIED OR STATUTORY, INCLUDING WITHOUT LIMITATION ANY WARRANTIES OF MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE. ROCKWELL AUTOMATION EXPLICITLY DISCLAIMS ALL WARRANTIES OF NON- INFRINGEMENT AND EXPRESSLY DOES NOT WARRANT THAT THE PRODUCTS, IN WHOLE OR IN PART, WILL BE ERROR FREE OR FREE FROM SECURITY VULNERABILITIES. IN NO EVENT SHALL ROCKWELL AUTOMATION BE LIABLE FOR (i) LOST PROFITS, LOST SAVINGS, DOWNTIME, SPECIAL, INDIRECT OR CONSEQUENTIAL DAMAGES OF ANY KIND, OR (ii) ANY PERSONAL INJURY, PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE ARISING OUT OF OR IN CONNECTION WITH THIS AGREEMENT, WHETHER IN AN ACTION IN CONTRACT, STRICT LIABILITY OR IN TORT INCLUDING NEGLIGENCE. 6. COMPANY AGREES TO INDEMNIFY AND HOLD ROCKWELL AUTOMATION HARMLESS FROM ALL COSTS, AWARDS, DAMAGES, EXPENSES AND FEES (INCLUDING ATTORNEYS FEES) RESULTING FROM OR RELATED TO ANY THIRD-PARTY CLAIMS (INCLUDING EMPLOYEES AND AGENTS OF COMPANY) AGAINST ROCKWELL AUTOMATION, ITS DISTRIBUTORS, AGENTS, OFFICERS, DIRECTORS OR EMPLOYEES FOR PERSONAL INJURY (INCLUDING DEATH), PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE RELATED TO OR RESULTING FROM THE USE OF THE PRODUCTS. 7. In the event a Product is exported, Company agrees to comply with all applicable United States Export Control Law and Regulations, and the applicable export control laws of other countries. This Agreement shall be governed by the laws of the state of Wisconsin. This Agreement is the complete and exclusive Agreement between Rockwell Automation and the Company, and supersedes all prior agreements, whether written or oral, relating to the Products.
AHIC NEED HELP ICON VF.png

Need Help?

If you need help with an application or have feedback from the Innovation Center, please contact us.

 

How can I make it work?

  • Hardware
    • Personal computer
  • Software
    • FactoryTalk Optix
    • Studio 5000
    • FT Echo
  • Background knowledge 
    • Knowledge of programming and configuration in FT Optix and Studio 5000.
 
 
 
 
 
 
 
 
AHIC STEP ICON.png

Implementation Guide

This document is divided into two parts, two configurations are needed. One for FT Optix and the Studio 5000 configuration.

First we will configure Studio 5000.

 
AHIC STEP ICON.png
 

Part I. 

Use Rockwell Automation Device Libraries in Studio 5000 Logix Designer

Prerequisites

  • Basic knowledge of Studio 5000 Logix Designer.
  • An existing project already created.
  • (Recommended) Studio 5000 Application Code Manager (ACM) installed to speed up the configuration process.
     
  1. Step 1.1
  2. Step 1.2
  3. Step 1.3
  4. Step 1.4
  5. Step 1.5
  6. Step 1.6
Open All Close All
Step 1.1
 

1. Download the Device Libraries

  • Go to the Rockwell Automation Download Center: rockwellautomation.com.
  • Search for “Device Library” and download the required libraries.
  • (Optional) Download Studio 5000 Application Code Manager (ACM) if you haven’t already.
  • This free software simplifies and accelerates device library configuration.
  • It acts as an extension of Logix Designer for bulk project configuration.
     
Step 1.2
 

2. Register the Library in Application Code Manager (ACM)

  • Locate the setup command file in the root folder of the library.
  • Run the script to automatically register all library objects in ACM.
  • Once the script is completed, close the window.
     
Step 1.3
 

3. Import Library Objects Using the Import Library Objects Plugin

In your Logix Designer project, right-click on any Task.
Select Plugins → Import Library Objects.
The Library Object Import Wizard will open this is a lightweight version of ACM inside Logix Designer.


On the left panel, you’ll see your list of registered libraries (those for which you ran the setup script).
Inside ralib device folder, you’ll find all Rockwell Automation device library objects.
Common folders include power discrete devices, network devices, etc.

For example, open the Power Motion folder and drag Kinetix 5500 device into the right panel under Library Objects.

You can drag multiple devices or instances if you wish to configure them in one import process.

 

kinetix-primer-integration_Imagen 1.jpg

kinetix-primer-integration_Imagen 1

Step 1.4
 

4. Configure Object Parameters

In the Object Configuration window, fill out the object parameters:

  • Name → The instance name for the AOI.
  • Description → A short helpful text that appears in the AOI description field and HMI faceplates.

Use the dropdowns to select the Task and Program where the routine will be imported.

Under Tag Scope, choose whether to create Program Scope or Controller Scope tags.

For some power device objects, configure Object Interface Data Type:

If using a PlantPAx system with a P controller, select Predefined Data Type and Controller Scope tags.

Set Include Hardware as needed:

  • True → The wizard automatically creates and configures the device module in the IO Tree.
  • False → If you already have the module, make sure it matches the required definition in the Device Library Reference Manual.

Verify the generated Module Name do not use the same name as the AOI.

kinetix-primer-integration_Imagen 2.jpg

kinetix-primer-integration_Imagen 2

Step 1.5
 

5. Complete the Import Wizard

In the Linked Libraries tab, click Auto Create to generate all required components.

Click Next to review pending changes.

Unless specific modifications are required, proceed to Finish.

Once the import completes: The module appears in the IO Configuration Tree.

A new routine is created with a rung containing the AOI instance and all required tags.

The code should compile without errors — no manual programming needed.
 

kinetix-primer-integration_Imagen 3.jpg

kinetix-primer-integration_Imagen 3

Step 1.6
 

6. Integrate Custom Logic

Device AOIs include interface tags used to connect your own control logic:

  • CMD (Command) → Used to control device outputs (e.g., Start, Jog, Locate LED).
  • STS (Status) → Provides status feedback (faults, warnings, connection, etc.).
  • SET (Settings) → Used for configurable parameters (e.g., Speed Setpoint, Trip Setpoint).
  • INF (Information) → Transfers data between related objects (e.g., between Power Device and Extension, or Safety Device and Group).

Do not write directly to module output tags that are already linked to an AOI.

When using PlantPAx or MachineBuilder instructions, they will automatically write to these control interfaces.
 

kinetix-primer-integration_Imagen 1.jpg

kinetix-primer-integration_Imagen 1

kinetix-primer-integration_Imagen 2.jpg

kinetix-primer-integration_Imagen 2

kinetix-primer-integration_Imagen 3.jpg

kinetix-primer-integration_Imagen 3

 
 
 
AHIC STEP ICON.png
 

Part II.

Use Device Libraries with FactoryTalk Optix

Prerequisites

  • FactoryTalk Optix Studio v1.4 or later installed.
  • Rockwell Automation libraries downloaded from the Product Compatibility and Download Center (PCDC).
     
  1. Step 2.1
  2. Step 2.2
  3. Step 2.3
  4. Step 2.4
  5. Step 2.5
  6. Step 2.6
Open All Close All
Step 2.1
 

1. Download and Install the Device Library

Go to Rockwell Automation’s PCDC website.
Search for the FactoryTalk Optix Library and verify version compatibility.

Download the latest release package.

Run the provided setup script to automatically copy library files to the default user library location.

The script prepares content for both FactoryTalk Optix Studio and Studio 5000 Application Code Manager.

Step 2.2
 

2. Import Library Objects into the Project

Open FactoryTalk Optix Studio and create or open a project.

For a new project: Enter a project name. Choose the display size. Click Create.

Organize your structure:

  • In the UI folder, right-click → Add Subfolder.
  • Rename it to match the library name using the edit icon.
  • Open the Libraries Window using the toolbar icon.

The window lists all available libraries from the default path (including those installed earlier).

Select the new library to filter its components.

Drag-and-drop the desired library component into your new subfolder.

The folder now contains:

  • Device faceplates
  • Graphic symbols
  • Private elements (panels, widgets)
  • Help panels

If you need multiple device objects and a “Conflicting Types Detected” dialog appears, choose:

  • Skip All → to keep existing types.
  • Replace All → to update to a newer version.
  • Rename All → to create alternate type names.

 

kinetix-primer-integration_Imagen 4.jpg

kinetix-primer-integration_Imagen 4

Step 2.3
 

3. Copy and Configure the Style Sheet

In the UI folder, add a new subfolder named Style Sheets.

Re-open the Libraries Window and select the Style Sheets Library.

Drag the ISA Style Sheet into your new Style Sheets folder.

 

This style sheet follows ISA-101 HMI standards and is recommended for consistent visualization. Close the Libraries Window.

 

Under the UI folder, select Native Presentation Engine.

In its Properties, set Style Sheet = ISA Style Sheet.

 

kinetix-primer-integration_Imagen 5.jpg

kinetix-primer-integration_Imagen 5

Step 2.4
 

4. Configure the Communication Driver and Import Tags

If no station exists yet, open the Dashboard → Configure Communications to Devices.

  • Click New Station.
  • Choose RAE EtherNet/IP Station → Next.
  • Enter the Controller Path and IP Address in the Root Property.
  • Confirm with Next → the new station appears under Available Devices.
  • Select the Configured Station in the Communication Drivers folder.

In its properties:

  • Set Enable Extended Properties = True.
  • Toggle Online Mode for tag import.
  • The Tag Import process starts automatically.
  • Review all detected controller tags.
  • Select All or only required tags → Next.

When import completes, the device appears with synchronized tag data.

Click Exit to close the wizard.

kinetix-primer-integration_Imagen 6.jpg

kinetix-primer-integration_Imagen 6

Step 2.5
 

5. Configure Graphic Symbols

In your UI folder, right-click the target window or screen → New → [Library Folder] → [Device].

Under Graphic Symbols, choose the desired representation: Text Button or Graphic Button.

 

Link the symbol to its Add-On Instruction (AOI) instance: Select the button → set Reference Tag by browsing to the device object tag.

 

For Configuration Label:

Leave blank to auto-populate from tag description metadata, or Enter a custom string. Keep all other parameters as default.

 

kinetix-primer-integration_Imagen 7.jpg

kinetix-primer-integration_Imagen 7

Step 2.6
 

6. Save the Project and Create Runtime

When ready to test, click the Emulator drop-down → Local.

Press + to add a New Target Device.

Fill in:

  • Target Name
  • IP Address

Destination Path of the target Optix Panel
 

Run the emulation.

kinetix-primer-integration_Image 8.jpg

kinetix-primer-integration_Image 8

kinetix-primer-integration_Imagen 4.jpg

kinetix-primer-integration_Imagen 4

kinetix-primer-integration_Imagen 5.jpg

kinetix-primer-integration_Imagen 5

kinetix-primer-integration_Imagen 6.jpg

kinetix-primer-integration_Imagen 6

kinetix-primer-integration_Imagen 7.jpg

kinetix-primer-integration_Imagen 7

kinetix-primer-integration_Image 8.jpg

kinetix-primer-integration_Image 8

 
 
 
 

Kinetix Premier Integration

Version 1.2 - June 2026

 

 
 
AHIC White Logo
Subscribe!

Receive new app releases and other updates from the Innovation Center directly in your inbox.

I want to subscribe.
 
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Sup...
  3. Chevron LeftChevron Left Pro...
  4. Chevron LeftChevron Left Downloads
  5. Chevron LeftChevron Left Innovation Center
  6. Chevron LeftChevron Left Kinetix Premier Integration
Please update your cookie preferences to continue.
This feature requires cookies to enhance your experience. Please update your preferences to allow for these cookies:
  • Social Media Cookies
  • Functional Cookies
  • Performance Cookies
  • Marketing Cookies
  • All Cookies
You can update your preferences at any time. For more information please see our {0} Privacy Policy
CloseClose