Contact Information If Safety Option Failure Occurs
    If you experience a failure with any safety-certified device, contact your local 
Rockwell Automation®
 sales office or Allen-Bradley®
 distributor. With this contact, you can do the following:- Return the device to Rockwell Automation so the failure is appropriately logged for the catalog number that is affected and a record is made of the failure.
- Request a failure analysis (if necessary) to determine the probable cause of the failure.
For information about how to remove and replace a drive, see the documentation for the drive. 
Provide Feedback