Compatible Drives
    The Integrated Safety Functions option module is compatible with these drive products:
      
- PowerFlex®755 drives (v14.xxx or later)
- PowerFlex®755TL low harmonic drives (v4.xxx or later)
- PowerFlex®755TR regenerative drives (v4.xxx or later)
- PowerFlex®755TM common bus inverters (v4.xxx or later)
- PowerFlex®755TS drives (v11.xxx or later)
     IMPORTANT: 
    
The Integrated Safety Functions option module is not compatible with PowerFlex 753 drives.
Integrated safety functions are controlled via the embedded Ethernet port on the drive only. The 20-750-ENETR can still be used, but only in conjunction with the embedded Ethernet port by being in Tap mode (safety messages must go through the embedded Ethernet port on drive).
The following Add-on Profiles (AOPs) are needed depending on the drive and type of control used:
| Product | Standard Control | Integrated Motion | 
|---|---|---|
| 755 | v5.03 (or later) | v19.00.00 (or later) | 
| 755T | v5.04 (or later) | Future | 
| 755TS | v15.01 | Future | 
Provide Feedback