Receiving
Standard packaged
PowerFlex®
755T wall mount products are boxed and shipped as a whole unit. Standard packaged PowerFlex®
755T floor mount products are shipped upright as a whole unit or in shipping sections as required. See Shipment Sections for details on shipment configurations. Each unit or shipping section is bolted to a shipping skid with removable shipping cleats and is covered with clear plastic wrap. Protection is for upright shipping and is not waterproof or watertight.
Heavy duty/export packaging is similar to standard packaging, but uses a plastic wrap suitable for occasional light water-spray. In addition, wood framing and sheeting surround the unit or shipping section. Heavy duty/export packaging is not waterproof, watertight, or intended for long-term storage.
- Upon delivery of thePowerFlex®755T product, refer to the packing slip for sizes and exact shipping weights. The packing slip also lists the items that are included in the shipment.
- Inspect the shipment for damaged or lost items. If the packaging appears to be damaged, unpack the equipment for further inspection. Open the doors or remove covers and inspect the major components for signs of damage.PowerFlex®755T floor mount enclosures are equipped with a key-operated door latch. A double-bit door key is taped to the enclosure door.Key-operated Door Latch and Key
- If there is evidence of damage or loss, follow this procedure:
- Note on the delivery receipt that the equipment being received is damaged.
- Contact the carrier that made the delivery and schedule an inspection.
- Inform your localRockwell Automation®representative that the equipment is damaged.
- Retain all product packaging for review by the carrier.
For further assistance, contact yourRockwell Automation®representative.
Provide Feedback