Handling
Two methods of handling PowerFlex 755T cabinet mount products within the receiving facility are acceptable.
- Transport by lift truck
- Overhead lifting (crane or hoist)
PowerFlex 755T cabinet mount products must be handled in the upright vertical position. Failure to comply with this requirement can lead to internal component and enclosure damage.
ATTENTION:
Risk of injury or equipment damage exists.
Follow local codes and guidelines and your company safety procedures when you handle PowerFlex drive products.
To avoid personal injury and structural damage to the PowerFlex drive product, do not lift or move the equipment by any means other than what is described in this publication. PowerFlex drive products are top- and front-heavy.
The following guidelines are provided to help avoid personal injury and equipment damage during handling and to help stabilize the product during transport to the installation site.
- Keep the product bolted to the shipping skid to minimize possibility of tipping.
- The factory-installed structural angles must remain secured to the enclosure during handling. Structural angles provide lift points and help minimize flexing of the enclosure during handling.
- Handle thePowerFlex®755T product carefully to avoid damage to the enclosures and paint.
- Keep the product in an upright position.PowerFlex®755T products, frame 7 and larger, are not to be tipped or laid flat during handling.
Before moving the product, verify that the route is clear of all obstructions and that other workers are a safe distance away.
Provide Feedback