Preface
This manual provides procedures for the mechanical and electrical installation of
PowerFlex®
755T products with TotalFORCE®
control. This manual includes the basic steps to transport, position, and join the product
enclosures, to make internal electrical connections, to connect to the AC supply source and to
the motor, and to wire basic I/O.This manual provides instructions for an initial product installation. Assembly procedures in chapters 1...5 assume that supply power is not connected. Once the product is connected to a power supply, always verify that system power is not present before performing any work on the product. See safety-related practices that are contained in the publication NFPA 70E, Standard for Electrical Safety in the Work Place.
This manual is intended for two types of personnel:
- Qualified personnel familiar with handling heavy equipment.
- Qualified electricians or other personnel who have experience with electrical terminology, equipment, methods, and safety precautions.
The Additional Resources section is a directory of
Rockwell Automation®
publications that provide detailed drive information from wiring and grounding recommendations to troubleshooting and repair.Provide Feedback