Bypass Contactor Precaution

ATTENTION:
Risk of equipment damage exists.
An incorrectly applied or installed bypass system can result in component damage or reduction in product life. The most common causes are:
  • Wiring AC line to drive output or control terminals.
  • Improper bypass or output circuits not approved by Rockwell Automation.
  • Output circuits which do not connect directly to the motor.
Contact Rockwell Automation for assistance with application or wiring.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal