Prepare Input Bay or First Power Bay

Follow these steps for Frame 13…15 Drives and Bus Supplies.
  1. Locate the box or boxes that hold coils of fiber-optic cables.
    Drive section with boxed fiber-optic cables.
  2. Remove and discard packaging.
  3. Carefully uncoil the fiber-optic cables.
  4. Compare the cable labels with the corresponding figure in the Fiber-optic Cable Routing by Product and Frame Size.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal