Make Cabinet-to-Cabinet Connections

Follow this sequence of steps for all cabinet-to-cabinet connections.
  1. Apply the gasket in one continuous strip around the open end of the enclosure. Seam the gasket (A) at the approximate middle of the bottom of the enclosure.
    Gasket location for cabinet-to-cabinet connections.
  2. Align the enclosures that are to be joined.
  3. Bring the loose cabinet close to the placed cabinet.
  4. Feed any fiber-optic cables (B) into the loose cabinet as you draw the cabinets together.
    Aligning cabinets to be joined.
  5. Bring the aligned enclosures tight together.
  6. Remove the structural angles.
    Remove structural lift angles from cabinets.
    IMPORTANT: Make any final position and leveling adjustments before this step.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal