Join Enclosures
PowerFlex®
755T products that ship in multiple sections must be connected after the sections are in their final positions. The enclosures are connected together using the joining hardware that is provided.Each of the three types of enclosure connections is made in the same way.
- Entry wire bay to input bay
- Power bay to power bay
- Power bay to exit wire bay
See the Release Enclosure From Shipping Skid section for instructions on removing the
hardware that secures the enclosure to the skid.
Provide Feedback