Install Power Modules in the Enclosure
Install the power modules into the enclosure in the reverse order of removal.
When you install the fiber optic cables:
- Remove the transceiver from the fiber-optic connector port on the power layer interface circuit board.IMPORTANT: Minimum inside bend radius for fiber-optic cable is 50 mm (2 in.). Any bends with a shorter inside radius can permanently damage the fiber-optic cable. Signal attenuation increases as inside bend radius is decreased.
- Without bending the cable to a radius less than 50 mm (2 in.), fully insert the fiber-optic cable into the transceiver.
- Insert the transceiver and fiber-optic cable into the connector on the board, until you hear an audible 'click.'Be sure that both plugs are fully engaged and seated and that the swing arm is down.ItemDescriptionADo not touch greased connector.BRemove protective covers only as needed.
Provide Feedback