Fiber-optic Connections

Fiber-optic cables are routed and connected at the factory in frame 8 and 9 drives and frame 8…10 bus supplies. These cables connect the fiber interface circuit board to the line side converters and motor side inverters in the adjacent enclosures.
IMPORTANT: Do not remove protective covers from unused wire harnesses, circuit board connectors, terminal blocks, and fiber-optic ports. Removing a protective cover can lead to contamination.

Control Pod to Power Module Connections

Fiber-optic cables at the control pod plug into transceiver modules that are mounted to a transceiver board. Transceiver boards plug into an edge connector on the fiber interface board. Inspect these connections at installation. Re-seating these connections after shipping and handling or after extended storage is recommended.
Image with callouts showing transceiver board connections at the fiber interface
            board and power layer interface board.
Item
Description
A
Transceiver boards plug into the fiber interface board. Verify that these connections are secure.
B
Fiber-optic cables routed from the control pod plug into the CTL transceiver cages that are mounted on the power layer interface boards located behind the power module access panel.
C
Fully insert fiber-optic cable plugs into the transceiver. Insert the transceiver into the connector cage on the power layer interface board until you hear it click into place.
D
Remove protective covers only as needed to help maintain corrosive gas protection.
E
Do not touch the greased connector to help avoid contamination.
F
Fully insert fiber-optic cable plugs into the transceiver. Insert the transceiver into the connector cage on the transceiver board until you hear it click into place.
G
Power module.

Fiber-optic Interface Board

The fiber-optic interface board holds the fiber transceiver circuit boards.
Fiber-optic Transceiver Circuit Board Connections
Image with callouts identifying the individual transceiver ports.
Port Name
Description
ACP0
Fiber transceiver port for the fiber-optic connection from ACP0 on the AC precharge control board.
ACP1/TAM
Fiber transceiver port for the fiber-optic connection from ACP1 (frame 13 and larger) or TAM on the torque accuracy module.
L0…L9
Fiber transceiver ports for the fiber-optic connections from CTL on the power layer interface board in power modules that are used as line side converters.
M0…M9
Fiber transceiver ports for the fiber-optic connections from CTL on the power layer interface board in power modules that are used as motor side inverters.
Each fiber-optic cable connects to its designated CTL port on the power module power layer interface circuit board.
Fiber Interface to CTL Port Connections
Image with callouts identifying the fiber Interface to CTL port connections.
Item
Description
A
Shipping split location.
B
Fiber-optic interface board connections.
C
L0-CTL and L1-CTL connections are made at the factory.
D
L2-CTL…L9-CTL connections.
E
M0-CTL…M9-CTL connections.
Fiber-optic cables are routed between cabinets through the power control channel. Cable guides are provided to help you keep the cables separated and organized.
Power Control Channel and Cable Guides
Image with callouts showing fiber-optic cables in the power control channel and cable
            guides organizing the cables.
Item
Description
A
Typical fiber-optic cable routing through the power control channel between cabinets.
B
Use cable guides to organize cable runs.
Cables are routed to the right-to-left oriented cabinets through the pass-through grommet that connects the wire bays in back-to-back configurations.
Fiber-optic Cable Routing Between Back-to-Back Entry Wire Bays
Image with callouts showing fiber-optic cable routing between back-to-back entry wire
            bays.
Item
Description
A
Back-to-back configured entry wire bays.
B
Pass-through grommet.
C
Power control cable channels.
D
Cable tie anchor points help to keep cables in place.
Cables are routed out of the power control channel and are plugged into the CTL transceiver port of the corresponding power module.
This image shows an 800 mm (31.5 in.) wide converter power bay. The front panels are omitted to show the proper cable path to the CTL transceiver port on the power layer interface board.
Power Bay Fiber-optic Cable Routing
Image showing fiber-optic cable routing from power control channel to the power
            module CTL transceiver port.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal