Configure Hardware Enable Circuitry
Each main control board has one digital input. Digital Input 0 can be used as a general-purpose programmable input, or by removal of a jumper, it can be configured as a dedicated hardware enable, which is unaffected by parameter settings.
- PowerFlex®755T - Digital Input 0 is found on TB1
To configure Digital Input 0 as a dedicated hardware enable, complete the following steps.
- Access the control pod.
- Locate and remove ENABLE Jumper on the Main Control Board (see diagram).
IMPORTANT:
Change main control circuit board configurations only when the control pod is de-energized.
Provide Feedback