Component Removal Requirements

This section outlines which components must be removed to install each
PowerFlex®
755T floor mount product. Each figure illustrates the minimum requirement to allow adequate access to join and anchor the enclosures, and to interconnect busbars. All modules can be removed however to improve access during installation. With all modules removed, it is easier to place, align, join, anchor, and interconnect the enclosures.
For instructions on how to remove these components from the enclosure, see the following sections.
  • Remove Frame 7 Power Module
  • Remove Frame 8…15 Power Module
  • Remove Frame 7 LCL Filter Module
  • Remove Frame 8…15 LCL Filter Module

Designated Component Positions

IMPORTANT: LCL filter modules and power modules are labeled to indicate their designated position in the product enclosure. Always reinstall modules in their corresponding factory-designated position. Make note of these labels during component removal. See the following figure for label locations.
LCL Filter Module and Power Module Position Labels
Image that shows the position of the corresponding position labels for roll-in modules.
Item
Description
A
F0 Label on Control Bus Assembly
B
F0 Label on LCL Filter Module
C
L0 Label on Control Bus Assembly
D
L0 Label on Line Side Power Module
E
M0 Label on Control Bus Assembly
F
M0 Label on Motor Side Power Module
G
Control Bus Assembly

LCL Filter Module Position Designation Labels

This table provides the possible position designation labels for LCL filter modules.
LCL Filter Module Labels for Frame Size
Frame Size
7
8
9
10
11
12
13
14
15
F0
F0
F0
F0
F0
F0
F0
F0
F0
F2
F2
F2
F2
F2
F2
F4
F3
F4
F4
F5
F6
F5
F7
F9
Early Production LCL Filter Module Labels for Frame Size
Frame Size
7
8
9
10
11
12
13
14
15
LCL0
LCL0
LCL0
LCL0
LCL0
LCL0
LCL0
LCL0
LCL0
LCL1
LCL1
LCL1
LCL1
LCL1
LCL1
LCL2
LCL2
LCL2
LCL2
LCL3
LCL3
LCL3
LCL4
LCL5

Temporary Component Storage

During installation, it is recommended that you designate a secure temporary storage area for the components that you remove from the enclosure. LCL filter modules and power modules present a tip-over hazard when removed from the enclosure. Measures must be taken to be sure that modules are stored in such a way that they do not pose a hazard.
Do not store components in active isles or work areas. A dedicated area that is designated for the temporary storage of the components that are removed during the installation process is recommended. Loose components can be hazardous and easily damaged.

Recommended Equipment and Accessories

Equipment is available that is designed to help you safely handle major components. The following equipment is recommended:
  • PowerFlex 750-Series module service cart, catalog number 20-750-MCART1, publication 750-IN105
  • PowerFlex 755T DC precharge module lift, catalog number 20-750-MCART2, publication 750-IN105
  • PowerFlex 750TM power and LCL filter module storage hardware, catalog number 20-750-MINV-ATIP, publication 750-IN106
  • PowerFlex 755T power module service ramp, catalog number 20-750-MRAMP1, publication 750-IN108
IMPORTANT: The service ramp is used only with power modules when the cabinet is mounted directly to the floor. Do not use the ramp to remove LCL filter modules from the cabinet. Review service ramp instructions before using.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal