Remove Other Modules from the Controller Chassis

If modules other than those modules listed in Redundant Chassis Requirements are in the controller chassis, you must remove them to convert to redundancy system. Not all components are compatible with all redundancy system revisions. To make sure of component compatibility, see the release notes for your redundancy system revision in the Product Compatibility and Download Center at rok.auto/pcdc.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal