Controller Diagnostics with the Logix Designer Application

A warning symbol appears in the controller organizer next to the I/O module under these conditions:
  • If there are faults or other conditions in the I/O module
  • If the connection to the I/O module fails while in run mode
When the I/O module is configured to cause a major fault on the controller and an I/O module fault occurs, the following can result:
  • Controller state displays Faulted.
  • Controller status displays Controller Fault and blinks red.
  • I/O module status displays I/O Not Responding and blinks green.
When the I/O module is not configured to cause a major fault on the controller and an I/O module fault occurs, the following result:
  • Controller state displays the current state, for example, Rem Run.
  • Controller status displays Controller OK and is steady green.
  • I/O module status displays I/O Not Responding and blinks green.
I/O Fault on the Controller
This image shows how to view an I/O fault on the controller.
IMPORTANT:
Safety Consideration
You cannot configure safety connections to automatically fault the controller
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal