Linear Topology

A linear network topology is a collection of devices that are daisy chained together across an
EtherNet/IP
network. Devices that can connect to a linear network topology use embedded switch technology to remove any need for a separate switch, as required in star network topologies.
Linear Network Topology Example
This image shows the controller in a linear network topology.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal