Controller Logging

The controller log stores various security-related events that can be written to a memory card or accessed via
FactoryTalk® AssetCentre
or a third-party syslog collector. Some of these events are Logix Designer application request errors, control system events, backup/restore events, and configuration changes.
For more information on how to access the controller log, see the Logix 5000 Controller Information and Status Programming Manual, publication 1756-PM015.
For more robust logging and to help prevent rollover, use
FactoryTalk® AssetCentre
or a syslog collector.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal