Create a Fault Routine
To create a fault routine, do the following.
- In the Controller Organizer, right-click the program and click Add > New Routine.
- On the New Routine dialog box, in the Name field, type a name for the fault routine.
- In the Type field, use the default setting, Ladder Diagram.
- In Program or Phase field, select the program or phase where the routine will reside.
- In the Assignment field, select Fault.
- (optional) Select the Open Routine checkbox, to open the ladder logic program immediately.
- Click OK.
Provide Feedback