Generate a CSV template to create FactoryTalk Smart Object instances
FactoryTalk Smart Object
instancesGenerate a CSV template that contains the columns required for creating
FactoryTalk Smart Object
instances.After using the CSV template to create
FactoryTalk Smart Object
instances quickly, import the new FactoryTalk Smart Object
instances into Studio 5000 Smart Object Configurator
.
TIP:
The generated CSV template differs from the CSV file that is created when exporting full configuration values. The generated CSV template does not contain read-only headings.
To generate a CSV template to create
FactoryTalk Smart Object
instances - SelectExport
. - InExport, selectCreation template.
- SelectExport.
- Select a folder and then type a name for the CSV file.
- SelectSave.An empty template appears in your folder.TIP: Files exported from the Smart Object Configurator application are unencrypted plain text that may contain sensitive information. You must ensure that the data is always secured, encrypted, and proper permissions are set to those files to prevent unauthorized modification. It is recommended that you store the files on local machine.
Provide Feedback