Bulk import FactoryTalk Smart Object configuration values
After exporting and then updating
FactoryTalk Smart Object
configuration values in a CSV file, bulk import the updated FactoryTalk Smart Object
configuration values to Studio 5000 Smart Object Configurator
.To bulk import
FactoryTalk Smart Object
configuration values- SelectImport
. - SelectEdit existing.FactoryTalk Smart Objectinstances
- SelectImport.
- Select a file.
- SelectOpen.The changes to the configuration values appear in the information model.TIP:InStudio 5000 Smart Object Configurator, enter values for a Periodic trigger in seconds. When importing configuration values from a CSV file, enter the Periodic trigger in milliseconds in theUpdate Rate (in ms)column.
Provide Feedback