Create a model
Create as many models as required for your
FactoryTalk Smart Object
information model.To create a model
- Perform one of these actions:
- To add the first information model, selectAdd
and then select Information model. - Right-clickInformation modelsand then selectNew information model.
- Set these basic properties:
- Name:Name of the model. See Rules for names and backing tags.
- Backing tag:Name of the backing tag in the controller. A backing tag is created in theStudio 5000 Logix Designerproject that contains the configuration information for theFactoryTalk Smart Object.
- Program:Controller program where the model resides.
- Routine:Controller routine where the model resides. The routine is ladder logic.
- Insert at:Location to add a rung in the routine where theFactoryTalk Smart Objectappears.
- Insert at end:Location at the end of the routine where theFactoryTalk Smart Objectappears.The code appears inStudio 5000 Logix Designer.
- SelectAdd.
Provide Feedback