Add a user-defined data type to an information model
Add a user-defined data type (UDT) to a
FactoryTalk Smart Object
information model. Set the basic collection properties to describe how the UDT FactoryTalk Smart Object
collects data.Configure UDTs in
Studio 5000 Logix Designer
before adding them to Smart Object Configurator. Use Studio 5000 Logix Designer
to make changes to UDTs.To add a user-defined data type to a
FactoryTalk Smart Object
information model- Perform one of these actions:
- Right-click a node and then selectNew UDT.
- Select a node, selectAdd
, and then selectUDT.TheAdd UDTdialog box appears.FactoryTalk Smart Objectinstances
- Set these basic properties:
- Name: Choose a UDT pre-configured inStudio 5000 Logix Designer.
- Backing tag: Name of the backing tag in the controller. A backing tag is created in theStudio 5000 Logix Designerproject that contains the configuration information for theFactoryTalk Smart Object.
- Source value tag (optional): Location where the data gathers.
- Program: Controller program where the node resides.
- Routine: Controller routine where the node resides.
- Insert at: Location to add a rung in the routine where theFactoryTalk Smart Objectappears.
- Insert at end: Location at the end of a routine where theFactoryTalk Smart Objectappears.
- Set these data collection parameters:
- On parent or periodic: When this checkbox andOn programmaticcheckbox are clear, data collection for this data value does not occur.TIP:It is possible to have multiple triggers active at once.
- Parent: When Parent is triggered, theFactoryTalk Smart Objectis also triggered.
- Periodic: Interval in seconds when data is sampled in the source tag.
- On programmatic: Ladder logic that triggers the condition for collection.
- SelectAdd.A new rung appears in the ladder logic. The UDTFactoryTalk Smart Objectappears in theFactoryTalk Smart Objecttree.
See also
Provide Feedback