Upload a project from an online controller or terminal
Upload a project from an online controller or terminal to create a new project file that is identical to the project in the controller or terminal.
To upload a project from an online controller or terminal:
- SelectFrom Upload.
- In theUpload From Controller or Terminaldialog box, type or browse to the path of an online controller or terminal.
- Select the controller or terminal.
- SelectUpload.
Provide Feedback