Upload From Controller or Terminal dialog box

Use the Upload From Controller or Terminal dialog box to upload a project from the controller or terminal.
IMPORTANT:
Use this dialog box to upload controllers and terminals for version 21.00.00 and later of the application.
To upload From Controller or Terminal dialog box
  1. Verify the path to where the selection will be uploaded.
    To change the path, select the down arrow to choose a new location.
  2. Select a supported controller or panel to upload.
  3. Select
    Upload
    to upload from the controller or terminal.
To open the
Upload From Controller or Terminal
dialog box, in the Studio 5000 launcher, under
Open
, select
From Upload
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal