Open an existing project file
Open an existing project file to modify or continue creating a runtime application or layout.
To open an existing project file:
- SelectExisting Project.
- (optional) In theOpen Projectdialog box, next to theFile namebox, select a file type from the list.
- In the project list, select a project file.
- SelectOpen.
Provide Feedback