Open an existing FactoryTalk View project

Open an existing project file to continue creating a
FactoryTalk View
runtime application.
To open an existing
FactoryTalk View
project:
  1. Select
    Existing Project
    .
  2. (optional) If
    Existing Project
    displays a list of options, select
    FactoryTalk View
    Project
    .
  3. In the
    Open
    FactoryTalk View
    Project
    dialog box, select an
    Application Type
    .
  4. Select an existing project.
  5. (optional) Select a language for the
    FactoryTalk View
    project.
  6. Select
    Open
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal